What are the hardware requirements for using the Vive Virtual Reality package in Process Simulate?
Solution
In the V14.1.1 Process Simulate documentation, there is a section on the Vive hardware and software requirements.
Open the Online Help, and browse to the first page under Process Simulate ->
Process Simulate Virtual Reality.

Then also, go to the Manufacturers page (https://www.vive.com/us/setup/), and hover over the Products on the top menu banner. Select the "Vive Ready" icon on the menu below the banner. You should see the recommended hardware specifications for Vive or Vive Pro. Also, see the complete list of graphic cards supported link (on that page) for more information.
There is also a button for "Test My PC". You can either run the program directly, or right-click on the button and download ViveCheck.exe for later use. This program will check the PC for compatibility with the Vive hardware and software.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: TECNOMATIX
Application: PROCESS_SIMULAT
Version: V14.1.1.X
Function: APPLICATIONS
Ref: 001-9292825