Tecnomatix Legacy Robcad is not using the full screen for display

2021-10-07T00:01:25Z
Robcad

Summary


Details

Installed Robcad successfully, and it is running. However, the program is only 
using about 80% of the display screen size. What could be the issue?


Note, the Display scale is at 125%.



Solution

All Tecnomatix progams should be running at 100% display scale.


Exit Exceed, change the display scale to 100%, and run Robcad again.


Result: The display of Robcad now takes up the full screen.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: TECNOMATIX
Application: ROBCAD
Version: V11.0RX
Function: INSTALL

Ref: 001-9292819

KB Article ID# PL8006770

Contents

SummaryDetails

Associated Components

Robcad Base