Origin of a Dimension is always Centered and cannot be moved

2021-10-06T23:26:30Z

Summary


Details

Origin of a Dimension is always Centered and cannot be moved.


Solution

This is caused by the Arrowhead Workflow, Automatic Orientation being toggled
ON. Toggling this OFF will allow placement of the dimension, or the origin
editing to be other than Centered.

Assure this is toggled OFF in the Template Part File in the Drafting
Preferences before creating a New Drawing.
Toggle this OFF in the existing Part File in the Drafting Preferences before
creating Dimensions.
For existing Dimensions, edit the Settings of each Dimension and toggle this
OFF.


Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 2008_R2
Product: NX
Application: DRAFTING
Version: V12.0.2
Function: ANNOTATION

Ref: 001-9291638

KB Article ID# PL8006768

Contents

SummaryDetails

Associated Components