Can not open more than one study at a time in Process Simulate

2021-10-07T00:01:25Z

Summary


Details

I can open one study, but when I open the second study, the second replaces the first study.

Solution

Process Simulate does not work like Microsoft Word where you can have several documents open at the same time. Process Simulate will only allow one study to be open at a time.  

The only work around would be to have Process Simulate open more than one instance,  with each open application supporting one study.  The only problem there is requiring the Options / Disconnected and Options / General / Library Root pointing at the same sysroot folder in each open application.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: TECNOMATIX
Application: PROCESS_SIMULAT
Version: V_UNKNOWN
Function: APPLICATIONS

Ref: 002-8006761

KB Article ID# PL8006761

Contents

SummaryDetails

Associated Components