NX Variable Guiding Curve subtype does not show up

2021-10-06T23:26:30Z
NX for Manufacturing

Summary


Details

Can not find the subtype Variable Guiding Curve while using the Mill Multi-Axis type template. 

Solution

On many occasions, the customer default •use updated template • (under File --> Utilities --> Customer Defaults --> Manufacturing --> General) is not checked and this will prevent the system to use the latest template part.  This will prevent the Variable Guiding Curve subtype to show since it is a new option in NX 12. 

Notes

KB Article ID# PL8006657

Contents

SummaryDetails

Associated Components

Manufacturing General