Impossible to publish SESP Workflows in SharePoint Designer

2021-10-06T23:53:11Z

Summary


Details

After upgrading Solid Edge and Solid Edge for SharePoint from ST8 to ST10 it is not possible to publish Solid Edge for SharePoint Workflows with SharePoint Designer 2013 if the workflow contains an "IF" action. 


The Error "Errors were found when compiling the workflow. The workflow files were saved but cannot be run." occurs.



Solution

This Problem does not only happen with Solid Edge for SharePoint Workflows but also with out-of-the-box "IF" actions and is caused by a .NET Security Update.


The behavior can be solved via a PowerShell script which adds the necessary types to all web applications' web.config files. 


Check out the web link for more information and details to create the script:
 
https://support.microsoft.com/en-us/help/4465015/sharepoint-workflows-stop-after-cve-2018-8421-security-update 


The script can solve the problem on SharePoint 2010 and SharePoint 2013. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110MP10
Function: SESP-WEB

Ref: 001-9276684

KB Article ID# PL8006625

Contents

SummaryDetails

Associated Components