Solid Edge Installing Solid Edge 2019 FlexNet License Manager on Windows 2008 R2.

2021-10-06T23:53:11Z
PART/SHEETMETAL SETUP

Summary


Details

Unable to install the Solid Edge 2019 FlexNet License Manager on a Windows 2008 R2 Server.

After copying the "Solid_Edge_DVD_ENGLISH__2019.exe" to the Windows 2008 R2 Server, trying to execute the software, it flashes and then disappears without any messages.

 

Solution

This could be related to a Windows 2008 R2 blockage issue. Since the file came from another computer it was being blocked from running or executing the Solid Edge install program. If you perform a right mouse click on the Solid Edge ".exe" and select the unblock option the program will execute as it should.





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 2008_R2
Product: SOLID_EDGE
Application: SETUP
Version: V219.0
Function: LICENSING

Ref: 002-8006606

KB Article ID# PL8006606

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES