In NX 12.0 there was a "Specify Origin Curve" option introduced in the "Section" group of the extrude menu.

What is this option used for?
Solution
The "Specify Origin Curve" option allows you specify which of the selected curves in the section string is the first curve in the extrude section, regardless of the order in which the curves were selected. The location and direction of the first curve of each section string is marked by a direction vector.
Specify Origin Curve is a function shared with Revolve. In Extrude command this ability only comes to play during Replace Feature mapping operations. where it helps to organized the mapping visually. Bringing more stable feature updates after feature remapping.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DESIGN
Version: V1872
Function: FEATURE_MODEL
Ref: 001-9277068