Is the Solid Edge 2019 License Manager compatible with Windows 2016 server?
In the readme this platform is not listed:
Solid Edge License Manager Operating System Information
FlexNet Publisher 2016 (11.14.0) is supported only on the 64-bit versions of
the following operating systems:
Windows 10
Windows 8
Windows 7 Ultimate
Windows Vista Ultimate
Windows Server 2008, Windows Server 2008 R2, Windows Server 2012, or Windows
Server 2012 R2
Solution
Solid Edge 2019 License Manager should work without issue on Windows Server 2016
Notes
If you have further inquiries about floating Licensing please refer to the FAQs collection link below:
Solid Edge Floating License FAQs Collection