Switching the Arrowhead Side from In to Out on Radial dimensions is not very efficient

2021-10-06T23:26:30Z

Summary


Details

When creating / editing Radial dimension it takes a lot of clicks and menu navigation to change the Arrow Orientation from In to Out and vice versa. 



Solution

The quickest way to switch the Arrow Orientation between In / Out is to use the right-hand mouse button menu option 'Arrowhead Orientation - In / Out', rather than using command 'Settings' dialog.


Note that the 'Arrowhead Orientation' menu option is only available when the 'Radial Dimension Settings - Line/Arrow - Arrowhead - Workflow - Automatic Orientation' option is OFF. (This can be set using the Custom Default 'Drafting - General/Setup - Standard - Customize Standard - Drafting Standard - Common - Line/Arrow - Arrowhead - Workflow - Automatic Orientation'.)

Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: DRAFTING
Version: V11.0.2
Function: DIMENSION

Ref: 001-9277460

KB Article ID# PL8006561

Contents

SummaryDetails

Associated Components