Callouts do not synchronize to the TC BOM View Revision FindNo anymore.
How to fix this?
Solution
Open Component Properties --> Tab Attribute..
- Interaction model Traditional
- Apply to: Component
- Select attribute CALLOUT
![](/kbassets/PL8006485/49c0e6ae35a5591b0aaca8590a468350b765f47e259ebb316ecfc9fbc8f6.jpg)
Delete this Component-level attribute, and the Instance-level will appear again. This attribute will synchronize to the BVR.
![](/kbassets/PL8006485/bb4831899e644b2ad9ab9b769dae09f735b9751ab44e9506540042c72812.jpg)
![](/kbassets/PL8006485/7684672b9f7338e2211471823bf989a470732d1bc2547252e88b4f598638.jpg)
The CALLOUT attribute only synchronizes the INSTANCE-level value to the BVR Findno. When the CALLOUT value is overruled at
COMPONENT-level (Apply to) then this will not synchronize to the BVR. Also, be aware that only the first-level components will synchronize to the BVR. Callouts for components in subassemblies are synchronized to the BVR of the subassembly.
![](/kbassets/PL8006485/004fd13e797545448e00834b9339a7744aae545ae4f77780f03f7875fb09.jpg)
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: XP64_SP2
Product: NX
Application: NXMANAGER
Version: V11.0
Function: ATTRIBUTES
Ref: 001-8394175