NX Errors during tool path generation

2021-10-06T23:26:29Z
NX for Manufacturing

Summary


Details

An error message is received when generating a milling operation. 

This dialog only includes an 'OK' button, with no option to view the exact warnings in the info window. 

The dialog does say to list the path to see the problems, something similar to:

---------- Diagnostic Information ---------- 

---------- Object Name: GROOVE_MILLING --------------- 

Warnings were produced during tool path generation. 

List the tool path to see the location and details. 

Solution

As noted in the general warning message, the tool path listing will report the problem points right in the path. The warnings indicate that some points in the path are below the Lower Limit Plane, i.e.

FEDRAT/IPM,10.0000 

GOTO/4.7500,-1.7458,0.9250 

PAINT/COLOR,31 

GOTO/4.7500,4.6614,0.9250 

PAINT/COLOR,37 

GOTO/4.7500,5.6614,0.9250 

$$ WARNING POINT IS BELOW LOWER LIMIT PLANE 

PAINT/COLOR,211 

RAPID 

GOTO/4.7500,5.6614,2.5000 

$$ WARNING POINT IS BELOW LOWER LIMIT PLANE 

PAINT/COLOR,186 

RAPID 

GOTO/4.7500,-2.7458,2.5000 

PAINT/COLOR,211 

RAPID 

GOTO/4.7500,-2.7458,0.8000

This is due to having a lower limit plane defined in the parent MCS. The operation is producing tool location points in the path that are below this lower limit, so NX is giving the warning. To resolve this, simply edit the Lower Limit Plane in the active MCS parent and reset this back to the 'None' option to disable this parameter (or adjust the existing lower limit plane downwards until the path will all be above it in space). 

Notes

KB Article ID# PL8006458

Contents

SummaryDetails

Associated Components

Manufacturing General