How the allocation or arrangement can be done for the scrap station numbers

2021-10-06T23:26:29Z

Summary


Details

Steps to reproduce.
Scrap station numbers will be set automatically.

Question.
Can we manually changing the station number during scrap creation or arrange them as required?



Solution

When creating scraps, user can assign its station number.

The default of Station Number is 1.
If user specify the value, the scrap will be positioned into the corresponding station when we use Strip Layout.
But if user doesn't specify the station number when creating scrap, all scraps' station number is 1.  When use Strip layout, all scraps will be positioned into station 1.


Now we can select a scrap in Strip Layout Navigator and then MB3, select Move Down number, the selected scrap will move to corresponding station.

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: KDA
Version: V12.0.2
Function: PROGRESSIVE_DIE

Ref: 002-8006423

KB Article ID# PL8006423

Contents

SummaryDetails

Associated Components