Titleblock is populating ItemRev 00 as a dash (-)

2021-10-06T23:26:29Z

Summary


Details

Cells in a table that reference the ItemRevision show as a dash (-) when the revision is 0 or 00. 



Solution

When the revision is zero ("0" or "00"), the cell can report a dash (-) instead if using the following setting: 
1. Highlight the cell in the table, 'MouseButton3-->Settings'. 
2. Expand 'Common' and highlight 'Cell'. 
3. Zero Display is set to: Dash (-) 
 Toggle this to "Zero Display = Zero". 
4. OK the Settings dialog.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V11.0.2
Function: PREFERENCES

Ref: 001-9270615

KB Article ID# PL8006420

Contents

SummaryDetails

Associated Components