When using the Measure command, measuring for instance a solid body, the report does not include any error estimate for area/volume/mass/etc. calculations.

Where can this be found?
Solution
By default the error estimates are not shown. You need to turn "Error Estimates" on in measure preferences. It is found under Measurements, Body tab, at the end of the list.

The result from a measurement will then look like:

Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DESIGN
Version: V1872
Function: INFO_ANALYSIS
Ref: 002-8006390