Cannot add new Holder using Electrode Design

2021-10-06T23:26:29Z

Summary


Details

When attempting to add a Holder in the Electrode Wizard, the message: "The 
fixture template does not exist in Teamcenter. Make sure the name is correct 
and the template has been imported into Teamcenter." is returned.



Solution

This is caused by having the Reference toggled ON in the Electrode Fixture 
dialog Settings. Toggle this OFF and the Holder should be added fine. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: NX
Application: KDA
Version: V12.0.1
Function: ELECTRODE_DESGN

Ref: 001-9267994

KB Article ID# PL8006353

Contents

SummaryDetails

Associated Components