Solid Edge Solid Edge 2019 Illustrations Exporter Add in is missing

2021-10-06T23:53:05Z
Apps Design

Summary


Details

The Add In ribbon with the Solid Edge 2019 Illustrations Exporter is missing in Solid Edge.



Solution

After the Installation of Solid Edge Technical Publications the independant Solid Edge 2019 Illustrations Exporter Add In is also installed and will be listed as an Add In in the Add In Manager, but it has no Add In ribbon User Interface. 


The Exporter is implemented into the "Save As" translation capabilities. 


To use this translator go to Solid Edge Application Button and run the "Save As" command. In the Filter pulldown list you will see "Solid Edge Illustrations (*.qsm)" 

Once you select the .qsm extension on the save as Dialog , the Options button is enabled and you can click and set your needed properties. 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: TECH_PUB
Version: V219MP1
Function: 3D_PUBLISHING

Ref: 001-9261028

KB Article ID# PL8006337

Contents

SummaryDetails

Associated Components

Technical Publications