Is there a way to externalize sketch feature when it is created using sketch section of extrude?

2021-10-06T23:26:29Z

Summary


Details

Steps to reproduce


  1. Create a new file.
  2. Select extrude command and create sketch using "Sketch Section". 
  3. Apply
     -> The sketch feature is internalized.



Question.


Is there a way to externalize sketch feature when it is created using sketch section of extrude?



Solution

The modeling preferences only controls the behavior when the sketch is not created via section.
If you create sketch and then extrude as two independent steps, then we have a choice to make the sketch go internal or stay external.


If we create extrude and then sketch via the section, it stays internal and there is no preference to change this default behavior.
We should select extrude from part navigator, and right click and pick Make Sketch External.



Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764
Product: NX
Application: DESIGN
Version: V11.0.2
Function: SKETCHER

Ref: 002-8006296

KB Article ID# PL8006296

Contents

SummaryDetails

Associated Components