When running an automation script from the journal tool in NX, is it possible to display a non-modal WinForms dialog?
Solution
No, the problem here is that once the form is displayed, execution is handed back to the journaling tool, which then proceeds to complete without hesitation. To display a non-modal WinForms dialog you must at least run from a compiled .dll.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: SYSENG
Version: V1859
Function: NXOPEN
Ref: 001-9264642