Can the function "Open Unmanaged Part" be turned off and disabled in NX12.0.1+

2021-10-06T23:26:28Z

Summary


Details

Can the function "Open Unmanaged Part" be turned off and disabled in NX12.0.1+?


NX12.0.1 introduced a new functionality to enable the managed mode of NX to open and work with prt files from the OS.


https://docs.plm.automation.siemens.com/tdoc/nx/12.0.2/nx_help/#uid:index_whatsnew:xid718414:xid1473234


Is there a way to turn off and disable this functionality? 

Solution

Set the following environment variable to turn off and disable this functionality:


UGII_DISABLE_NATIVE_LOAD_IN_MANAGED_SESSION=1

Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: XP64_SP1
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: FILE_OPEN

Ref: 001-9262255

KB Article ID# PL8006233

Contents

SummaryDetails

Associated Components