How to fix a Synchronous Sheetmetal part so it will edit.

2021-10-06T23:53:02Z

Summary


Details

Is there anything that can be done to "fix" a Synchronous sheetmetal part when edits are always failing with error messages?



Solution

1. Save the test case model out to Parasolid and then read it back in as a 
.par Part file 
2. Now in the part environment perform a Copy Surface/Chain Option and copy 
all the internal surfaces of the part, including loops (holes & cutouts) 
3. Delete the Body Feature and Thicken the chained surface body to the desired 
 sheet metal thickness 
4. Switch to Sheet Metal and utilize the Thin Part to Sheet Metal command to 
 transform the part to sheet metal now providing sheet metal attributes to the 
 model 
5 Your flange can now be moved and additional flanges can be added to the 
existing ones 
6. Since you no longer have the Features from the previous model, you can just 
 use Recognize Holes to get the hole attributes back 
7. This now is a workable Synchronous model and only takes a few minutes to do 



Notes and References





Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 10_1703
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V219.0
Function: SYNC_EDIT

Ref: 001-9259271

KB Article ID# PL8006166

Contents

SummaryDetails

Associated Components