Details
Prior to NX12.0.1, image can be captured via File > Export > PNG, JPEG, GIF, TIFF or BMP. Now these commands are not available under File > Export.
How to capture image of graphic window in NX from NX12.0.1 + ?
Solution
There is a new command under File > Export called Image. This launches Export Image dialog which user can specify the type of format.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: SYSENG
Version: V12.0.1
Function: VISUALIZATION
Ref: 002-8006156