Simcenter 3D Solutions NXMotion - how to create a torque depending on time and torsion angle

2021-10-06T23:26:28Z
Simcenter 3D

Summary


Details

At X time step enable a torque load on a rotary joint which varies with the angular displacement (for example 0Deg = 1Nm, 10Deg = 3Nm, 20Deg = 2Nm, 30Deg = 0.5Nm, I have complete torque vs angular displacement graphs to input in reality) then at time step Y turn this load off allowing the component to return to its starting position by means of another external load which is constantly applied (EG a spring force).

I can easily apply a torque VS time load as is mentioned below, and I can put a torque vs angular displacement load onto a rotary joint however I cannot disable this load to allow the component to return to its home state.

Solution

I created a torque that varies with the rotation angle. That also depends on time. After a defined time its value goes to zero.

Please carefully analyze the formula into torque T001.

the formula that defines its value is:

IF(time-t_stop:IF(AZ(J002_i,J002_j)-10:1+0.2*AZ(J002_i,J002_j),1+0.2*AZ(J002_i,J002_j),IF(AZ(J002_i,J002_j)-20:3-0.1*(AZ(J002_i,J002_j)-10),3-0.1*(AZ(J002_i,J002_j)-10),2-0.15*(AZ(J002_i,J002_j)-20))),0,0) 

The "IF" functions requires 4 parameters.

the first is the condition, the following are the values returned if the condition is below, equal or above zero.

First one is about time: "time-t_stop" time is the independent variable of the solver, t_stop is a user defined variable to set the time when the torque must go to zero.

the following three parameters refer to values of "time-t_stop" below zero, equal to zero and above zero.

So if "time-t_stop" < 0 then the angle value is checked: IF(AZ(J002_i,J002_j)-10, where AZ(J002_i,J002_j) is the angle value of the link on which the torque is applied. If the angle is below 10 degres (that is AZ(J002_i,J002_j)-10 < 0) then the torque value is:1+0.2*AZ(J002_i,J002_j). If the angle is equal to ten, again, the value is 1+0.2*AZ(J002_i,J002_j).

if the angle is above 10 the a new check is performed: IF(AZ(J002_i,J002_j)-20. If the angle is below 20 degres (that is AZ(J002_i,J002_j)-20 < 0) then the torque value is:3-0.1*(AZ(J002_i,J002_j)-10). If the angle is equal to zero, again, the value is 3-0.1*(AZ(J002_i,J002_j)-10). If no other check is satisfyed, that means that the angle is above 20 degress and the torque value is 2-0.15*(AZ(J002_i,J002_j)-20)).

If time is equal or above t_stop, the torque value is zero.

Notes

KB Article ID# PL8006049

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow