How can I run Power Drafting in NX 11.0?
There is no shortcut available to start NX in Power Drafting mode.
Solution
NX Power Drafting the product and functional control in NX existed up to and
including NX 9.0. In NX 10.0 and beyond it is replaced by NX Layout.
So for instance in a NX11 standard installation there is a NX start shortcut
named "NX11.0 Layout" which is the equivalent to Power Drafting.
To manually run NX in Layout mode run the following command: ugraf.exe -layout
Inside a standard NX session there is also a "Layout" role that will limit NX
menus to what NX Layout product offers.
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 764
Product: NX
Application: GATEWAY
Version: V11.0
Function: LAYOUT
Ref: 001-9248270