NX Routing Path Length can't be measured with the new 'Measure' of 12.0.1 MP1

2021-10-06T23:26:28Z
NX for Design

Summary


Details

The length of branching path was easily measured with 'Routing Path Length'


But Routing Path Length can't be measured with the new 'Measure' of 12.0.1 MP1.


How to measure Routing path length with the new measure command of 12.0.1 MP1



Solution

Using "Object set" and "Point" objects in the new measure command, the intended routing path selections and its measurements can be achieved.



Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: DESIGN
Version: V12.0.2
Function: INFO_ANALYSIS

Ref: 002-8005994

KB Article ID# PL8005994

Contents

SummaryDetails

Associated Components

Modeling