Part file is opened by NX viewer not by NX Application

2021-10-06T23:26:28Z

Summary


Details

Once NX viewer is launched and closed, Double clicking on a part file causes the part gets opened only in NX viewer not in NX application.



Solution

Start -> Run- > regedit


 
Expand "HKEY_CLASSES_ROOT\UGpartfile\shell\open\command"


 
Set the following value data to (Default) Value Name according to your installation path.


 
"C:\apps\NX12\NXBIN\ugs_router.exe"  -ug -use_file_dir  "%1" -version=V30.0 -opts –nx


 
Now the part should be opened in NX instead of viewer.



Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: ASSEMBLIES
Version: V12.0.1
Function: PART_FILE_OPS

Ref: 002-8005993

KB Article ID# PL8005993

Contents

SummaryDetails

Associated Components