Details
When the component is moved, the display position of measure distance dimension is far away from the model measured if the component is made as displayed part.
However the dimension is displayed as created when the component is made as work part.
Solution
The recommended procedure is to create the associate measurement from where (assembly context or component) the user is going use most of the time.
This behavior is improved from NX12.0.1MP1 with the new measure command
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: DESIGN
Version: V10.0.3
Function: INFO_ANALYSIS
Ref: 002-8005990