PMI Display in multi-selected Views

2021-10-06T23:26:27Z

Summary


Details

In order to display a PMI in certain model views, you can right click  a PMI display instance and choose "Display"-> "in Views".

Being in "Display in views" dialog window and having multi-selected the target views you want the PMI to be displayed in, you should be able to choose whether to activate them by check marks or by selecting "Enable" from the context menu (RMB on the selected views).

But using the context menu method ("Enable"), you get only ONE of the multi selected views activated




Solution

The behavior of Enable/Disable in Display In Views... with multiple selection is working as designed. 

To change the visibility of multiple selected views at once, use the checkboxes.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: PMI
Version: V11.0.2
Function: DISP_ALL_VIEWS

Ref: 002-8005920

KB Article ID# PL8005920

Contents

SummaryDetails

Associated Components