Simcenter 3D Solutions Difference between Log & Octave in Y-axis options of "Acoustic Power" graph

2021-10-06T23:26:27Z
Simcenter 3D

Summary


Details

What is the difference between Log & Octave in Y-axis options of "Acoustic Power" graph

After creating graph of "Acoustic Power" with Nastran OP2 files-Sort2 Results

It seems the value of Y-axis in Octave is same as Log.

Solution

In such a graph, the only difference between log and octave may be the axis tags. 

You can see the differences in the tags when changing to 1/3-octave or 1-12 octave axis. 

However, octave band axes should only be used in a frequency axis and are typically used together with octave band summation.

Notes

KB Article ID# PL8005848

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow