Details
Coloring information is not inherited by the mirrored feature when source part is exchanged.
Possible workflow:
"Edit with Rollback" on a existing feature and exchange input link to an other one.
The mirrored feature will keep its old color information (green). You have to delete the mirrored feature and set it again
Expectation is, that the coloring information has to be inherited by the mirrored feature.
Solution
This is working as desingned:
Mirror (and Pattern) features only inherit colors from master features, during create operation.
Reapplying master color for every update of Mirror, will wipe out any Mirror
specific colors.
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V11.0
Function: FEATURE_MODEL
Ref: 002-8005841