NX What is the advantage of using tc_publishing_utility over traditional save?

2021-10-06T23:26:26Z
NX for Design

Summary


Details

What is the advantage of using tc_publishing_utility over traditional save?

Solution

Use the new tc_publishing_utility command line utility to publish NX part data to Teamcenter. The utility opens the part or assembly, publishes the data to Teamcenter, and then closes the part. The part itself is not saved to Teamcenter. 

This is useful in publishing the released data as well.

Notes and References

IR 9215528

Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: UTILITIES

Ref: 002-8005752

KB Article ID# PL8005752

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX