What's -publish_jt in tc_publishing_utility?

2021-10-06T23:26:26Z

Summary


Details

What's -publish_jt in tc_publishing_utility?

Solution

o Import or create a simple assembly in managed mode.
o This assembly has few components with geometry in component levels.
o Make sure not to have "Save JT Data" set to ON.
o Make sure NOT to check Publish Optional Information during import 
o Fire the following command 
tc_publishing_utility -u=username -p=password -publish_jt=yes -part=@DB/ItemID/RevID -load_a=yes -bypass=no

This will publish JT datasets in Teamcenter.
This is useful to generate JTs for existing parts where JTs are not present.

Notes and References

IR 9215528

Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: UTILITIES

Ref: 002-8005747

KB Article ID# PL8005747

Contents

SummaryDetails

Associated Components