Details
What's -publish_we in tc_publishing_utility?
Solution
o Import or create a simple assembly in managed mode.
o This assembly has few components between which a welding joint is created in a component level
o Make sure NOT to check Publish Optional Information during import
o Fire the following command
tc_publishing_utility -u=username -p=password -publish_we=yes -part=@DB/ItemID/RevID -load_a=yes -bypass=no
This will publish welds in Teamcenter.
Notes and References
IR 9215528
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 764SP1
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: UTILITIES
Ref: 002-8005746