Details
Adding a new "Note" [Mandatory ] in the custom symbol which is already registered Library, the text of a placed custom symbol is initialized by Update the symbol.
Solution
In the Custom Symbols, if we add or delete any Note, existing Custom Symbol Note gets overwritten, but modifying the Note there are no changes in the custom symbols.
Workaround:
---------------
User need to be add both "Arbitrary" as well as "Mandatory" Note initially while creating Custom Symbol and then modify the text as per the requirement.
the text of a placed custom symbol cant initialized by Update the symbol.
----------------
Notes and References
9239872
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: DRAFTING
Version: V11.0.2
Function: SYMBOL
Ref: 002-8005725