Details
Cannot return a borrowed license that was borrowed with the previous version
of Solid Edge.
Solution
Borrowed licenses of Solid Edge do not actually capture the license file from the license file it borrows from. But because the install of your license manager has been updated, the return borrow license will not work and the new version of Solid Edge is not getting checked out because the borrowed license
is for a previous version. So you need to clear the borrowed license to stop you from getting the message. When you connect to the network you will be able to use the new version, but disconnected from the network the client still sees the old borrowed license of the previous version and fails.
Do the following:
On the client machine:
1. Run regedit.
2. Locate registry HKEY_CURRENT_USER->software->FLEXLM License Manager->Borrow
3. Delete this Registry to remove the encryption string that represents the
borrowed license.
4. Reboot your machine
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 10_1703
Product: SOLID_EDGE
Application: SETUP
Version: V219.0
Function: LICENSING
Ref: 001-9245586