Can not display the project ID column in the Solid Edge Save as dialog

2021-10-06T23:52:59Z

Summary


Details

Can not display the project ID column in the Solid Edge Save as dialog window.

Solution

If no project is assigned to user who is logged in then project ID column will be not shown.


To see the project ID in the column of the Solid Edge Save as dialog for logged in user must define project in RAC and add that user into that project.



Notes and References

9238648

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V219.0
Function: SEEC

Ref: 002-8005685

KB Article ID# PL8005685

Contents

SummaryDetails

Associated Components