NX Spreadsheet error - Excel is not installed on this machine. Using ONLINE Excel

2021-10-06T23:26:26Z

Summary


Details

Error when trying to run NX Spreadsheet

     Spreadsheet
     Excel is not installed on this machine

Excel 2016
Excel Add-ins for NX were applied, but the NX Spreadsheet still fails with the above error.  

Solution

This user did not have Microsoft Office / Excel installed on the local machine.
Therefore the error message is to be taken at face value.

Development confirms
****************
We support the Online NX-Excel interaction. 
But if Excel is not installed locally on the workstation, 
the Online NX-Excel interaction is not possible.

Now Microsoft has come up with various flavors, like Office 365 (subscription model).
We support that also - but even for that, Excel must be installed locally on the workstation. 

****************

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: GATEWAY
Version: V11.0.2
Function: SPREADSHEET

Ref: 002-8005660

KB Article ID# PL8005660

Contents

SummaryDetails

Associated Components