How to edit the Material drop down list in the Moldwizard BOM?

2021-10-06T23:26:26Z

Summary


Details

How can users customize the Material drop down list shown in the Moldwizard BOM? 




Solution

Users can define the Material list in the Excel file which is located in either of these 2 locations:

MOLDWIZARD_DIR\templates\bom\Bom_Data\Bom_Data.xlsx

or

UGII_BASE_DIR\moldwizard\templates\bom\Bom_Data\Bom_Data.xlsx


Open the spreadsheet and select the "Material" sheet to access the Parameters section with the options.
Users may add or remove entries as necessary.

Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: KDA
Version: V12.0
Function: MOLDWIZARD

Ref: 001-9241757

KB Article ID# PL8005655

Contents

SummaryDetails

Associated Components