Details
When launching NX, the following error occurs:
*************
System cannot initialize callback interface
nx_mfgviewmaker_core.cm#class UGS::System::IconfigureCore
__ptr64 from library libmfgviewmakerinit
**************
This is machine specific - all other NX clients on site work fine (same installation methods performed).
Solution
Uninstalling and reinstalling NX on this particular machine solved the problem.
Notes and References
One case was found with this error message, concluded the machine hardware graphics combination to be UNSUPPORTED - per the Hardware (Graphics Card) Certification matrix.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764
Product: NX
Application: SYSTEM
Version: V11.0.2
Function: WNT_INSTALL
Ref: 002-8005648