Simcenter 3D Solutions Avoiding 'group' labelling conflicts in '.sim' and assembly fem '.afm' files

2021-10-06T23:26:26Z
Simcenter 3D

Summary


Details

New in Simcenter 3D 12, the 'grouping' functionality was enhanced such that the user can now assign and change labels when creating or editing a group (in previous releases the label was assigned automatically and could not be edited).  This change was implemented for all Simcenter 3D data files where groups can be created ('.fem', '.sim', '.afm' and assembly fem '.sim').

However, with the implementation of this new functionality, it was decided that there is now no point In having the software override labels assigned to groups associated with 'child' items (e.g. '.fem' file) in the context of a 'parent' item (e.g. '.sim' file) when new groups are created in the context of the 'parent' item. 

Hence the labels of groups associated with 'child' items are no longer automatically incremented and consequently the creation of new groups in the context of the 'parent' item can result in duplicate labels.

Solution

The assembly fem 'assembly label manager', which provides an automated way to avoid labelling conflicts within the context of an assembly fem, has been enhanced to include 'groups' as one of the modifiable entity types.

Additionally, a new 'simulation label manager' function has been introduced - this is similar to the assembly fem 'assembly label manager' function, but can be used to control the labels of specific entity types (coordinate systems, physical properties and groups) within the context of a '.sim' file.

***

With respect to this topic, reviewing the following articles within the Simcenter 3D 12 help documentation may be beneficial:

Group labels

Label management enhancement

Notes

KB Article ID# PL8005646

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow