About the logic of placement of WCS with 'CSYS of Object' Type.

2021-10-06T23:26:25Z

Summary


Details

1. Open an irregular shape part file in NX. 
2. Menu -> Format -> WCS -> Orient. 
3. In 'Type' select "CSYS of Object" 
4. Select the face which is irregular in shape. 
[OK] the 'CSYS' dialog. 
The WCS will be placed on the face (WCS may be placed outside of the face also depending upon the shape of the face). 
 
How is the WCS placed? What is the logic of placing WCS with 'CSYS of Object' Type?

Solution


"CSYS of Object" option places the WCS at the center of the planar face bounding area.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: GATEWAY
Version: V11.0.2
Function: WCS

Ref: 002-8005631

KB Article ID# PL8005631

Contents

SummaryDetails

Associated Components