NX NX: Can't extract NX 12.0.2?

2021-10-06T23:26:25Z
NX System Administration

Summary


Details

After downloading NX-12.0.2.zip, the file will not extract?

Solution

One reason this can happen is that beginning with NX 12, the maintenance releases were split into a
multi-part zip file. This can happen if all parts of the file are not present when extracting. Please make sure you've downloaded all three files:


 nx-12.0.2.z01 - 2,097,152,000 bytes - Jul 12, 2018 
 nx-12.0.2.z02 - 2,097,152,000 bytes - Jul 12, 2018 
 nx-12.0.2.zip - 1,761,874,306 bytes - Jul 12, 2018 


And then try to exract NX 12.0.2.ZIP. 

Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: NX
Application: SYSTEM
Version: V12.0.2
Function: WNT_INSTALL

Ref: 001-9241906

KB Article ID# PL8005627

Contents

SummaryDetails

Associated Components

Installation Licensing Plotting