Symbolica How to stop Additional Expressions being created for Interpart Expressions when opening part in NX10 or later

2021-10-06T23:26:25Z
Symbolica

Summary


Details

When a part containing interpart expressions created in a version prior to NX10  is opened in NX10 or later additional expressions appear in the part.  How can I stop these expressions being created?

Solution

It is an intentional change in NX11 that creates the additional expressions for the Interpart Expression values. This change was necessary to allow support for additional functionality whilst maintaining the correct relationships.

The article in the link below explains a bit more about this:

http://gtac.industrysoftware.automation.siemens.com/view.php?si=001-7335921

There is no method available to maintain the same number of expressions as in NX9.0. In order to display only the expressions of interest you can use the Options in the Visibility section of the dialog to filter ths list.
For example, turning Off "Show Locked Formula Expression" will remove the locked interpart expressions from the list.




 


 



Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: DESIGN
Version: V10.0
Function: EXPRESSION

Ref: 002-8005604

KB Article ID# PL8005604

Contents

SummaryDetails

Associated Components

Symbolica