Missing parts/bodies after SolidWorks (.sldprt) import

2021-10-06T23:52:58Z

Summary


Details

After importing a SolidWorks (.sldprt) file, many parts/bodies are missing.

Solution

In some cases, the SolidWorks "Assembly" is created using Multi-Body technology, similar to Solid Edge.
"Outside" of Solid Edge one way for verifying would be that there is only one ".sldprt" file, instead of an assembly file (.sldasm) and mutliple part files (.sldprt).

Usually the user has to enable multi-body import in Solid Edge, because by default this is turned off.  
Unfortunately this option is not shown in the import dialog, so the user has to manipulate the "SW2SE.INI" file manually.

Please make sure, that following line is included:


Import MULTI_BODY part files=1


This will add support for multi-body, and the imported part/assembly should be complete now.

Notes and References

IR#9236828

Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764
Product: SOLID_EDGE
Application: TRANSLATORS
Version: V219.0
Function: SW

Ref: 002-8005571

KB Article ID# PL8005571

Contents

SummaryDetails

Associated Components