ugmanager_clone.bat requires perl in TC_ROOT which is unavailable on client

2021-10-06T23:26:25Z

Summary


Details

ugmanager_clone.bat is a perl script.

Perl is not installed on 4-Tier Teamcenter clients, so the script does not run. 



Solution

1. install 2-tier Teamcenter client 
2. share TC_ROOT from server 
3. use ug_clone.exe directly with necessary arguments


e.g. as described for Template install in NX help: 
https://docs.plm.automation.siemens.com/tdoc/nx/12.0.2/nx_help#uid:tc_templates 
_install


Installing templates in a Teamcenter four-tier environment 
We recommend that you install the templates in a Teamcenter two-tier 
environment. If you are required to install in a four-tier environment, 
perform the following steps to install the templates. 
1. Ensure the following environment variables are set: 
o UGII_UGMGR_COMMUNICATION 
o UGII_UGMGR_HTTP_URL 
o UGII_BASE_DIR 
2. Enter the following from a Teamcenter command prompt: 
"%UGII_BASE_DIR%\ugii\ug_clone.exe" -pim=yes -u=infodba -p=infodba 
-o=import -dir="%UGII_BASE_DIR%\ugii\templates" -default_a=overwrite 
-default_n=autotranslate -aut=legacy -default_f=infodba:"NX Templates" 
-s=nxdm_template_import.clone"



Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: NXMANAGER
Version: V11.0
Function: CLONE

Ref: 001-8388449

KB Article ID# PL8005549

Contents

SummaryDetails

Associated Components