Arrowhead missing from Datum Feature Symbol in dxf viewed in Autocad

2021-10-06T23:26:25Z

Summary


Details

When translating a drawing to dxf, the arrowhead ("triangle") of GD&T symbols are missing.

-> Cannot see leader arrowheads!

Solution

This is AutoCAD limitation. AutoCAD does not display arrowheads if leader length is less. Please refer following link for more details:


https://knowledge.autodesk.com/support/autocad/troubleshooting/caas/sfdcarticles/sfdcarticles/Cannot-see-leader-arrowheads.html

"Leader arrowheads are not visible when the extension line of the leader is less than twice the size of the arrowhead. This is the expected behavior of leader arrowheads. To force arrowhead visibility, you must reduce the size of the arrowhead or increase the length of the leader extension line."


Workaround:
Datum symbols leader length can be increased by dragging it away from leader termination point.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: TRANSLATOR
Function: DXF_DWG

Ref: 002-8005546

KB Article ID# PL8005546

Contents

SummaryDetails

Associated Components