How to export an assembly "as saved" with ug_clone?

2021-10-06T23:26:25Z

Summary


Details

Export an assembly "as saved" using the ug_clone utility from TC11.2/NX10 with the following command seems not  working:


ug_clone -pim=yes -u=xxx -p=xxx -g=xxx -o=export -r=as_saved 
-asse=@DB/Testassy/00 -default_n=autotranslate -default_d=d:\temp

Results in error message:
ERROR: (943013) - Input revision rule does not exist.
        While setting revision rule as_saved







Solution

The error appears because of  "As_saved" is not a revision rule.


So if running ug_clone from a command or batch file this would require a load 
options file to be declared for the command line ug_clone.
There is no ug_clone utility to define this directly as the -r for a revision 
rule.
You can save the load options to a file when running NX with Teamcenter. 
File - Assembly Load Options - Save to File
All the setting are in the load_options.def file. This file can be saved to a 
folder for example D:\temp.


In the tc command prompt where you will run the ug_clone 


set UGII_LOAD_OPTIONS= d:\temp\load_options.def 

Now run ug_clone
e.g.:
D:\Software\NX\NX10\UGII>ug_clone -pim=yes -u=infodba -p=infodba -g=dba 
-o=export
-asse=@DB/Tesassy/A -default_n=autotranslate -default_d=d:\partsexportdirectoy

ug_clone Starting...
FCC interface version fms.10.1.0.20130514.00.
Loaded implementation library 
'D:\Software\TC\tccs\lib\FCCClientProxyDllv11064.dll'.
FCC Interface Implementation fms.10.1.5.20160212.00 initialized.
Logging export to export.clone
export completed successfully

Notes and References

7846690

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: NXMANAGER
Version: V11.0
Function: CLONE_EXPORT

Ref: 002-8005542

KB Article ID# PL8005542

Contents

SummaryDetails

Associated Components