Details
When a single Center Mark is created on a row of holes, the Center Mark is
hidden for all of the holes if a View Break is created that passes through the
row of holes.
Solution
When creating Center Marks on a row of holes the 'Create Multiple Center Marks' option should be selected, so that each hole has its own Center Mark. When a View Break is created that crosses the row of holes, only the Center Marks within the View Break will be hidden, and the Center Marks on the visible holes will remain.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: DRAFTING
Version: V11.0
Function: ANNOTATION
Ref: 001-8388335