How to enable assembly arrangement synchronization between NX and Teamcenter?

2021-10-06T23:26:25Z

Summary


Details

How to enable assembly arrangement synchronization between NX and Teamcenter?



Solution

To enable assembly arrangement synchronization between NX and Teamcenter during loading of an assembly, several customer defaults must be set. To do this, in the customer defaults in NX, choose Teamcenter Integration > General, select the Assembly page, then select the following:
 
- Structure Update on Load. Choose Complete or Add Components that have a Position.
 
- Synchronize Assembly Arrangements
 
- Update Modified Transforms

Notes and References

9153580 

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: NXMANAGER
Version: V11.0.2
Function: ASSEMBLY

Ref: 001-9153580

KB Article ID# PL8005511

Contents

SummaryDetails

Associated Components