Aborting out of Solid Edge when saving to a pdf format.

2021-10-06T23:51:50Z

Summary


Details

Aborting out of Solid Edge translating a Solid Edge file to a PDF format. 




Solution

This issue was found to be related to the Solid Edge Velocity PS Printer 
2.0, when saving to the PDF format. 



To resolve this issue you must remove both the Printer & Driver, removing only 
one of these options will resolve the problem.


Workflow Steps: 
- Uninstall Solid Edge 
- Uninstall the Printer & Driver, click Control Panel 
- Select Printers & Drivers 
 Delete the appropriate Printer, then proceed to remove the printer driver. 
 RMB click in free space under the Printers list and select Server Properties 
 Click Drivers tab 
 Remove the appropriate driver 
- Re-install Solid Edge and the problem should be resolved.



Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: SOLID_EDGE
Application: TRANSLATORS

Ref: 001-9094352

KB Article ID# PL8005347

Contents

SummaryDetails

Associated Components